Automatic Diagnostic Event Summary configuration
The
Automatic Diagnostic Event Summary Properties
dialog box contains tabs that are used to configure the appearance and operation of the Automatic Diagnostic Event Summary object at runtime:- GeneralUse theGeneraltab to change how information is displayed and how operators interact with the information.
- ColumnsUse theColumnstab to change which columns are displayed and to configure their appearance.
- Status barUse theStatus bartab to select the items that are displayed on the status bar and to change their tooltips.
- ToolbarUse theToolbartab to change the buttons that appear on the toolbar.
- SortUse theSorttab to sort the data displayed on the contents of different fields.
- SubscriptionsUse theSubscriptiontab to subscribe to events that match defined criteria.
- Display filtersUse theDisplayfilterstab to limit the data displayed based on defined criteria.
- BehaviorUse theBehaviortab to control how operators can interact with the Automatic Diagnostic Event Summary at runtime.
- StatesUse theStatestab to configure a distinct appearance for each of the event states.
Provide Feedback