Automatic Diagnostic Event Summary Properties - Status bar tab
How do I open the Automatic Diagnostic Event Summary Properties dialog box - Status bar tab?
- InFactoryTalk View Studio, add an Automatic Diagnostic Event Summary object to a display.
- Right-click on the Automatic Diagnostic Event Summary object, and then clickProperties.
- Click theStatus bartab.
Use the
Status bar
tab in the Automatic Diagnostic Event Summary Properties
dialog box to select the items that are displayed in the status bar and to change their tooltip.To change the appearance of the status bar, click the
General
tab.The following table describes the settings on the
Status bar
tab.Setting | Description |
---|---|
Show panel | Each item in the list represents a panel displayed on the status bar. To include an item on the status bar, select the corresponding check box. |
Icon | The icons shown in this column are read-only. |
Tooltip | Leave the default tooltip or type a different tooltip for each item on the status bar. At runtime, the Server Status tooltip is composed of Connected or Disconnected tooltip text, or both, followed by a colon and the area and server name. For example, Connected: Line1Area:Packaging Server. The tooltips must be configured at design time. |
Provide Feedback