Create a subscription (Diagnostics)
Create an event subscription to specify the subscription settings. The newly created subscription removes the default subscription, which includes all areas.
To create a subscription
- In FactoryTalk View Studio, open the display that includes the Automatic Diagnostic Event Summary object.
- Right-click the Automatic Diagnostic Event Summary object, and then clickProperties.
- On theSubscriptionstab, under theEvent subscriptionslist, clickAdd.
- Type a unique name for the new subscription.
- Under theScopeslist, clickBrowseto specify the scope for the events to subscribe to.TIP:The default scope is(Any scope), which is equivalent to selecting the top node in theSelect Scopebrowser.
- ClickOK.
Provide Feedback