Automatic Diagnostic Event Summary Properties - Subscriptions tab

How do I open the Automatic Diagnostic Event Summary Properties dialog box - Subscriptions tab?
  1. In
    FactoryTalk View Studio
    , add an Automatic Diagnostic Event Summary object to a display.
  2. Right-click on the Automatic Diagnostic Event Summary object, and then click
    Properties
    .
  3. Click the
    Subscriptions
    tab.
Use the
Subscription
tab in the
Automatic Diagnostic Event Summary Properties
dialog box to subscribe to events that match specific criteria.
If you do not create an event subscription, the Automatic Diagnostic Event Summary uses the default subscription, which displays all events as they occur in the
FactoryTalk
system.
If you create an event subscription, only the events that you subscribe to are displayed in the Automatic Diagnostic Event Summary.
The following table describes the settings on the
Subscriptions
tab.
Setting
Description
Event subscriptions
Displays the subscriptions currently configured for the Automatic Diagnostic Event Summary.
Add
Used to add a subscription.
Remove
Used to remove the subscription and stop filtering events on the subscription criteria.
Rename
Used to provide a new name for an existing subscription. All event subscription names must be unique.
Scopes
Identifies the scope used to determine the events forwarded to the Automatic Diagnostic Event Summary. A scope is a pre-defined area or group of events.
The default scope is
(Any scope)
, which is equivalent to selecting the top node in the
Select Scope
browser.
Browse
Used to subscribe to events that fall within a given scope.
Remove
Used to remove the selected scope.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal