Automatic Diagnostic Event Summary Properties - Column tab
How do I open the Automatic Diagnostic Event Summary Properties dialog box - Column tab?
- InFactoryTalk View Studio, add an Automatic Diagnostic Event Summary object to a display.
- Right-click on the Automatic Diagnostic Event Summary object, and then clickProperties.
- Click theColumntab.
Use the
Columns
tab in the Automatic Diagnostic Event Summary Properties
dialog box to change which columns are displayed, and to configure their appearance in the Automatic Diagnostic Event Summary.The following table describes the settings on the
Column
tab.Setting | Description |
---|---|
Add and remove columns in the event list | The columns across the top of the event list represent some of the data fields in the Automatic Diagnostic Event Summary. All of the data fields are shown in the detail pane, but you can select the ones you want to display in the event list. |
Reposition columns | To change the order in which columns are displayed in the event list, click a column name in the list, and then click Move Up or Move Down to move the column name up or down in the list. |
Change column heading text | To change the heading of a column, select the column name in the Heading text list, and then type a name in the text box.The text you type in the Heading text box does not replace the original name of the column in the column list, or on the Display filters or Sort tabs. |
Change column widths | Select the column name in the list, and then type a number in the Width box to change the width of columns in the event list. For example, increase the width of the column if you expect the text in the column to be long or vice versa. |
Change column alignment | Select the column name in the list, and then click the Align box to select the alignment in which you want the information to appear in the column. |
Change the format of information displayed in the columns | In the Format list, select the format for the information in the column. |
Show seconds for all timestamps | Click and select the timestamp type to be displayed in the Automatic Diagnostic Event Summary from the list:
Timestamps properties must be configured at design time. |
Provide Feedback