Automatic Diagnostic Event Summary Properties - Toolbar tab
How do I open the Automatic Diagnostic Event Summary Properties dialog box - Toolbar tab?
- InFactoryTalk View Studio, add an Automatic Diagnostic Event Summary object to a display.
- Right-click on the Automatic Diagnostic Event Summary object, and then clickProperties.
- Click theToolbartab.
Use the
Toolbar
tab in the Automatic Diagnostic Event Summary Properties
dialog box to change the buttons that appear on the toolbar in the Automatic Diagnostic Event Summary at runtime. To save space in the Automatic Diagnostic Event Summary, add only the toolbar buttons for features that operators frequently use.The following table describes the settings on the
Toolbar
tab.Setting | Description |
---|---|
Add and remove buttons on the toolbar | The toolbar buttons at the top of the Automatic Diagnostic Event Summary provide quick access to operations for operators. Add or remove the toolbar buttons as needed. |
Change button captions | To change the caption for a button, select the button name in the list. In the Caption box, type a caption for the button.Display properties must be configured at design time. If the caption is not visible on the button, select a different format for the button in the Format list. |
Change button tooltips | To change the tooltip for a button, select the button name in the list. In the Tooltip box, type a tooltip for the button.You can configure the tooltips as needed. Display properties must be configured at design time. To show tooltips, select the Tooltips check box on the General tab. |
Display images, captions, or both on toolbar buttons | To change how a button is displayed on the toolbar, select the button name in the list, and then choose the format to use. |
Provide Feedback