Restful APIs

Use the Application Programming Interface (API) to access the FactoryTalk System Status Portal information.
The following table identifies the general response states and codes for all Restful APIs.
Type
Value
Description
Response state
0
The data is valid.
1
The data is invalid.
2
The data has errors.
Response code
200
It is successful.
500
It is an internal server error.
501
The server process is starting.
601
Unable to verify FactoryTalk security.
700
Access is denied.
701
Unable to find the endpoint element.
900
Unable to validate the response data.
2400
Invalid parameter value for request
2500
The execution of the FactoryTalk Alarms and Events web server timeout expired.
2501
Unable to run requests on the FactoryTalk Alarms and Events web server.
2502
The FactoryTalk Alarms and Events web server has not finished starting.
2503
Unable to run the request on the FactoryTalk Alarms and Events web server.
2601
Unable to verify the FactoryTalk security token because it has expired, or it is invalid.
2602
Unable to see alarm data due to insufficient permission.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal