FactoryTalk System Status Portal
How do I open the
FactoryTalk
System Status Portal?
- In the web browser's address bar, enter one of the following:
- http://or<ComputerName>/FTSystemStatushttps://, where<ComputerName>/FTSystemStatusComputerNameis theFactoryTalkDirectory server computer. For example,https://.<MyFTDPC>/FTSystemStatus
- http://<IPAddress>/FTSystemStatushttps://, where<IPAddress>/FTSystemStatusIPAddressis the IP address of theFactoryTalkDirectory server computer. For example,https://.<192.16.2.1>/FTSystemStatus
TIP:If you are signing in from theFactoryTalkDirectory server computer, you can uselocalhostto replaceComputerNameorIPAddress. For example,http://localhost/FTSystemStatusorhttps://localhost/FTSystemStatus. - PressEnter.
- Enter aFactoryTalkuser account with access to the application that you want to view and its password. Select theKeep me signed incheckbox to stay signed in until you sign out manually or cookies stored by the website in your browser are deleted.
- SelectSign in.
FactoryTalk
System Status PortalFactoryTalk Administration Console
. This portal is installed with FactoryTalk Services Platform
by
selecting FactoryTalk
System Status PortalThe web portal shows the status of the following server types:
- HMI servers
- FactoryTalk Alarms and Eventsservers
- Data servers (FactoryTalk Linx, OPC UA, and OPC DA servers)
- FactoryTalk Historian SE and ME servers
- FactoryTalk® AssetCentreservers and agents
The application status will not be influenced by the FactoryTalk Historian SE server,
FactoryTalk Historian ME server, and FactoryTalk AssetCentre server and agent, because these
servers and agents do not belong to any FactoryTalk application. The icons show the health
of each application:
means that none of the servers in the application has issues.
means that at least one of the servers in the application has issues.
To switch to the black or white mode, select one of these icons from the upper-right corner
of the web page:
turns on the light mode.
turns on the dark mode.
Provide Feedback