View the status of an application

FactoryTalk
System Status Portal shows the status of all the applications and all the servers in the application, including HMI,
FactoryTalk Alarms and Events
,
FactoryTalk Linx
, OPC UA, FactoryTalk Historian SE and ME servers, and OPC DA servers, and standby servers if redundancy is configured.
TIP:
FactoryTalk
System Status Portal shows the server status of FactoryTalk Historian SE version 9.00.00 or later, which requires to select
System Status v9.00.00
during the FactoryTalk Historian SE installation.
To view the status of an application
  1. In
    FactoryTalk
    System Status Portal
    , enter a
    FactoryTalk
    Directory username with access to the application you want to view and its password, and then select
    Sign In
    .
  2. On the
    FactoryTalk Applications
    page, select an application.
  3. View the status of all the severs in the application in
    Group view
    or
    Titles view
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal