View FatoryTalk View SE client connection
FactoryTalk System Status Portal provides the historical record of each FactoryTalk View SE client connection, including the connected client name, IP address, begin-end time, duration, and connection history on all HMI servers.
TIP:
When HTTPS is enabled, the information of FactoryTalk View SE client connection is available.
To view FactoryTalk View SE client connection
- InFactoryTalk System Status Portal, enter a FactoryTalk Directory username with access to the application that you want to view and its password, and then selectSign In.
- On theFactoryTalk Applicationspage, select an application.
- Select a primary or secondary HMI server.
- (optional) Selectmoreā¦to view the connection history on all HMI servers, including the connected server, computer name, username, start time, end time, and process ID.TIP:Process IDis not shown on small screens, like mobile phones.
Provide Feedback