Server status of an application

After selecting an application on the main page, the
FactoryTalk
System Status Portal shows the status of all the servers in the application, including HMI,
FactoryTalk Alarms and Events
,
FactoryTalk Linx
, OPC UA, and OPC DA servers, FactoryTalk Historian SE and ME servers, and standby servers if redundancy is configured.
The following table lists the server statuses and their meanings.
Server status
Description
Active
The server is active and running.
Standby
The redundant server is in the standby mode in an active-standby pair.
Not loaded
The server is not currently in use and has not notified the system that it is running.
Failed
The server has failed. When redundancy is configured, the partner server provides service.
Transitioning
The server is changing from one state to another.
Unknown
The sever is in an unknown state.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal