Status of FactoryTalk AssetCentre server and agents
The following table shows the status of
FactoryTalk AssetCentre
server and
agents and the meanings.Server status | Description |
---|---|
Active | The server is running and connected. The agent is running a
schedule. |
Standby | The agent is in the idle state. It is only available for the
agent. |
Offline | The server or agent is disconnected, or the host computer is
turned off. |
Unknown | The server or agent is in an unknown state. |
Provide Feedback