AlarmSummary
Gets the alarm summary from FactoryTalk System Status Portal.
Request method
- GET
URI
- api/v1/alarm/summary/{serverName}
Parameters
The following table identifies the AlarmSummary parameters.
Parameters | Descriptions |
---|---|
ServerName | The target FactoryTalk Alarms and Events, OPC UA, or OPC DA server name |
Returned values
The following table identifies the returned values in JSON format.
Parameters | Descriptions |
---|---|
Data | It is an object including these properties:
|
Provide Feedback