Applications
Gets the current application list.
Request method
- GET
URI
- api/v1/applications
Parameters
The following table identifies the Applications parameters.
Parameters | Descriptions |
---|---|
Username | The FactoryTalk user account |
Password | The FactoryTalk user account's password |
Returned values
The following table identifies the returned values in JSON format.
Parameters | Descriptions |
---|---|
ApplicationList | It is an array object including these properties:
|
Provide Feedback