Occurrences

Gets the number and priority distribution of alarms in a period of time.
Request method
  • GET
URI
  • api/v1/alarm/top-api/v1/alarm/occurrences/{serverName}/{timeBegin}/{timeEnd}
Parameters
The following table identifies the Occurrences parameters.
Parameters
Descriptions
ServerName
The target FactoryTalk Alarms and Events, OPC UA, or OPC DA server name
TimeBegin
The begin time
TimeEnd
The end time
Returned values
The following table identifies the returned values in JSON format.
Parameters
Descriptions
Items
It is an array object including these properties:
  • Time
  • Ugent
  • Hign
  • Medium
  • Low
  • UTC Time
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal