Connections
Gets the HMI connections list from FactoryTalk System Status Portal.
Request method
- GET
URI
- api/v1/hmi/connections/{serverName}/{hostName}
Parameters
The following table identifies the Connections parameters.
Parameters | Descriptions |
---|---|
ServerName | The target HMI server name |
HostName | The HMI server computer's name |
Returned values
The following table identifies the returned values in JSON format.
Parameters | Descriptions |
---|---|
ConnectionList | It is an array object including these properties:
|
Provide Feedback