DBName

Gets the alarm database name from FactoryTalk System Status Portal.
Request method
  • GET
URI
  • api/v1/alarm/dbname/{serverName}
Parameters
The following table identifies the DBName parameters.
Parameters
Descriptions
ServerName
The target FactoryTalk Alarms and Events, OPC UA, or OPC DA server name
Returned values
It will return the database name.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal