TopStaleness

Gets the top 10 alarms with the longest active state duration in a period time.
Request method
  • GET
URI
  • api/v1/alarm/top-staleness/{serverName}/{timeBegin}/{timeEnd}
Parameters
The following table identifies the TopStaleness parameters.
Parameters
Descriptions
ServerName
The target FactoryTalk Alarms and Events, OPC UA, or OPC DA server name
TimeBegin
The begin time
TimeEnd
The end time
Returned values
The following table identifies the returned values in JSON format.
Parameters
Descriptions
Items
It is an array object including these properties:
  • AlarmName
  • Stale
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal