Work with shortcuts
Use shortcuts to pass properties to screens to customize the screen content that appears on the HMI device.
A shortcut is a link to a screen on which the shortcut is based. Shortcuts can be based on either new or existing screens.
Shortcuts based on existing screens can reuse screen content to create additional screens that are similar but have been customized to display different values. A project can contain up to 200 shortcuts.
Provide Feedback