Rename a shortcut

The default shortcut in a project is named Screen_001. Rename a shortcut to make the name more meaningful. For example, give the shortcut a name that reflects the purpose, content, or targeted user of the shortcut. Names within a folder must be unique and are not case sensitive. For example, Bottling_Line and bottling_line are considered identical names.
To rename a shortcut
  1. In the
    Project Explorer
    , expand the
    Navigation Menu
    folder.
  2. Click the shortcut once to select the item.
  3. Click the shortcut again and type the new name.
    TIP:
    Right-clicking the shortcut, selecting
    Rename
    , and then entering a new name also renames the shortcut.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal