Open the defining screen of a shortcut

Open the screen linked to a shortcut. From this defining screen, make changes to depict in the shortcuts of the defining screen.
To open the defining screen of a shortcut
  1. In the
    Project Explorer
    , expand the
    Navigation Menu
    folder.
  2. Point to the shortcut in the folder to identify the defining screen of a shortcut. The name of the screen linked to the shortcut appears in a tooltip.
  3. Right-click the shortcut and select
    Edit Definition
    . The screen on which the shortcut is based opens.
    TIP:
    Tips:
    • When a shortcut is open, select the link at the top of the shortcut to open the defining screen of the shortcut.
    • When both the defining screen and a shortcut of that defining screen are open, changes made to the defining screen do not appear in the shortcut until selecting the shortcut.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal