Shortcut tab
How do I open the Shortcut tab?
In the
.
Project Explorer
of the open project, expand the Navigation Menu
folder, and double-click the shortcut. Shortcut names are preceded by a Shortcut
icon The
Shortcut
tab displays the contents of the shortcut on the HMI device. A shortcut is a link to the screen on which the shortcut is based. A shortcut displays the same content as the screen to which it is linked. Create screen properties the shortcut can use to pass different tag values to a screen. This allows creating a reusable screen that multiple shortcuts can call using different tag values. Use shortcuts to provide operators:
- Quick access to a screen.
- A way to call the same screen with different data.
Use the
Shortcut
tab to: - Specify the icon for the shortcut to appear on theNavigation menuof the HMI device.
- Modify properties passed from the shortcut to the defining screen.
- Open the defining screen of the shortcut.
Provide Feedback