Change a user-defined property
After creating a user-defined property, it appears on the
Property Definition
tab and the Properties
tab for the screen or popup. User defined properties created for the definition of an Add-On Graphic appear on the Properties
tab for an instance of the Add-On Graphic. Use the Property Definition
tab to change the definition of a user-defined property. Use the Properties
tab to change the value of a user-defined property rather than the property itself.To change a user-defined property
- Select the screen, Add-On Graphic definition, or popup that contains the user-defined property to change.
- Make changes to the property:
- Use theProperty Definitiontab to change the Name, Data Type, Description, or Category of the user-defined property.
- Use thePropertiestab to change the value or binding.Changes to user-defined properties take effect immediately and are saved when the project is saved.TIP:A value or binding for an Add-On Graphic cannot change on thePropertiestab for the definition of an Add-On Graphic. Change a value or binding for an instance of the Add-On Graphic on thePropertiestab.
Provide Feedback