New Shortcut dialog box

How do I open the New Shortcut dialog box?
In the
Project Explorer
of the open project, right-click the
Navigation Menu
folder and click
New Shortcut
.
Use the
New Shortcut
dialog box to create a shortcut to a screen. Shortcuts provide quick access to a specific screen on the HMI device and can pass tag values from the shortcut to the defining screen using properties you create. Create a shortcut to create another version of a screen by changing the properties of the shortcut.
Shortcuts appear in the
Navigation Menu
folder of the
Project Explorer
. Shortcuts also appear in the
Navigation menu
on the HMI device.
Use the
New Shortcut
dialog box to:
  • Create a new shortcut.
  • Link a shortcut to a new or existing screen.
  • Open a new screen that is linked to the shortcut.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal