Configure an event to trigger an action

An event triggers an action on the HMI device. The operator on the HMI device or the system can trigger an event.
Events can be added and configured to trigger an action when a:
  • Graphic element behaves like a button
  • Graphic element or screen is pressed or released
  • Key on an external keyboard is pressed or released
  • Graphic element enters or exits a selected state
Graphic elements on the HMI device include Add-On Graphics.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal