Change a command that an event performs
Make changes to the command of an event after creating the event. For example, change the destination screen for a
Screen Navigate
command. Changing the type of event after creating the event is not supported. For example, changing a Touch Press
event to a Key Release
event is not supported. Delete an event if an event of that type is no longer required.
IMPORTANT:
If an event references a
State Table
and then the name of the table changes, change the reference to reflect the new State Table
name. View Designer
does not automatically update references with the new name.To change a command that an event performs
- Select the element or screen in theProject ExplorerorGraphic Explorer, or in theScreenarea.
- In thePropertiespane, select theEventstab.
- To the left of the event, selectShow/Hide
to expose the commands associated with the event. - Change the commands of the event. For example, change the expression, value, or destination of the command.
Provide Feedback