In what order are touch events triggered?

The order in which touch events trigger depends on the events configured for a screen and its graphic elements. When configuring multiple graphic elements or Add-On Graphics with touch events, touch events trigger for items in the following order:
  • Screen events
  • Group events
  • Graphic element events
    TIP:
    Tips:
    • Press events trigger before release events.
    • An overlay over a group or graphic element does not affect the events of the group or graphic element, unless the overlay has an event of its own. If an overlay has an event of its own, that event takes place rather than the event of the group of graphic element.
    • Events created for an instance of an Add-On Graphic take precedence over events created for a graphic element within the definition of the Add-On Graphic. If the same event type exists in both the definition of an Add-On Graphic and an instance of that Add-On Graphic, the event for the instance of the Add-On Graphic on the screen is performed on the HMI device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal