Example: Events for graphic elements below groups do not trigger
If a group lies on top of an input graphic element, touching the group triggers the event of the group. Pressing the input graphic element does not open a virtual numeric keypad or virtual standard keyboard.
In this example, a group that has an event associated lies on top of an input graphic element that is not part of the group.

Press Event | Triggered action |
![]() | Press here to trigger the event associated with the group. |
![]() | Press here to trigger the event associated with the group. |
![]() | Press here to trigger the event associated with the group. The virtual numeric keypad or the virtual standard keyboard does not open. |
Provide Feedback