Example: Group events trigger before events for input graphic elements open a keypad or keyboard
If a group contains line art and an input graphic element, the event of the group triggers regardless of the touch location on the group. Pressing the input graphic element triggers the event of the group and opens the virtual numeric keypad or virtual standard keyboard.
In this example, there is an event associated with the group. The group contains line art and a text input graphic element.

Press Event | Triggered action |
![]() | Press here to trigger the event associated with the group. |
![]() | Press here to trigger the event associated with the group. |
![]() | Press here to trigger the event associated with the group and then open the virtual numeric keypad or virtual standard keyboard to enable input. |
Provide Feedback