Events tab
How do I open the Events tab?
On the
Menu
bar, click View > Properties Window
, and click the Events
tab.Import the desired languages before changing the language that appears on the HMI device.
Use the
Events
tab to:- Add an event.Define what occurs to trigger an action. For example, add an event for when releasing a graphic button or key, or when pressing or releasing the screen or key. Add events typically performed by a button. For example, a Button Behavior event can configure a graphic element to act as a momentary push button or high-speed HMIBC button.Add events to a graphic element, Add-On Graphic, screen, popup, or the System Banner. For each event, configure the action that triggers when the event takes place. For example, an event of pressing a graphic element could trigger the action of opening a specific screen.
- Configure a command.Define the action triggered when the event occurs. For example, the command can log off the project, navigate to a screen, increment a value, or calibrate the HMI device screen for touch.
- Change the command an event performs. Delete the command and add a new command for the event.
- Delete a command.Delete a command from an event so the command does not trigger when the event occurs.
Provide Feedback