Delete an event

Delete an event or multiple events from the
Events
tab. Deleted events no longer perform on the HMI device screen.
To delete an event
  1. Select the graphic element, Add-On Graphic, or screen in the
    Project Explorer
    ,
    Graphic Explorer
    , or in the
    Screen
    area.
  2. In the
    Properties
    pane, select the
    Events
    tab.
  3. Next to the event, select
    Delete Event
    . The
    Events
    tab no longer lists the event.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal