Multiple events
Create multiple events of the same type to change the same property value for a graphic element or write to the same tag value. This shows only the result of the last event configured for the element. For example, create two events for a graphic element. One event changes the FillColor property of a bottle to white. The other event changes the FillColor property of the same bottle to yellow. The HMI device shows only the contents of the bottle that turn yellow.
Create multiple events that change a different property for a graphic element or write to a different tag value. This shows the result of each of the events for the graphic element. For example, create two events for a graphic element. One event changes the FillColor property of a bottle to yellow. The other event changes the CapColor property of the same bottle to gray. The HMI device shows the contents of the bottle turning yellow and the bottle cap turning gray.
Provide Feedback