Example event
To create an event, assume that a screen named
Bottling Line A
opens when the operator releases L10
on the physical keypad of the HMI device. To accomplish this: - Open the project containing theBottling Line Ascreen.
- Select the screen from which to navigate to theBottling Line Ascreen. Select the screen in theProject Exploreror theGraphic Explorer, or open theScreenand select its canvas.
- In thePropertieswindow, select theEventstab.
- Add an event and select aKey Releaseevent.
- Select theL10key as the key to prompt the event. When using an external keyboard instead of the physical keypad of the HMI device,L10corresponds with pressingShift+F10on an external keyboard.
- Add aNavigationcommand to the event and selectScreen Navigate.
- In theNavigate Tobox, select theBottling Line Ascreen to open when releasingL10on the HMI device physical keypad, orShift+F10on an external keyboard, from the currently selected screen.
Provide Feedback