Delete a command from an event
Delete a command to no longer have the event perform the command. For example, delete a navigation command from the event of a button to no longer have the
Touch Press
event of the button open a popup. To delete a command from an event
- Select the graphic element, Add-On Graphic, or screen in theProject Explorer,Graphic Explorer, or in theScreenarea.
- In thePropertiespane, select theEventstab.
- To the left of the event, selectShow/Hide
to display the commands associated with the event. - Next to the command in the card, selectDelete Command. The event no longer performs the deleted command. Deleting all commands means the event no longer performs any commands when the event triggers.
Provide Feedback