Alarm Import Export Wizard
How do I open the Alarm Import Export Wizard?
- Open theAlarmsfolder in theExplorerwindow.
- Right-clickAlarm Setupand selectImport and Exportfrom theContextmenu.
- If theAlarm Setupeditor is opened and has unsaved changes, a message appears asking if you want to save your changes.
- SelectYesto save your changes, close theAlarm Setupeditor and open the Alarm Import Export Wizard.
- SelectNoto close theAlarm Setupeditor without saving your changes and open the Alarm Import Export Wizard.
- SelectCancelto leave theAlarm Setupeditor open. The Alarm Import Export Wizard will not open.
An application's alarm configuration information is created in the application's
Alarm Setup
editor and is contained in a file called MachineAlarms.MAL.Use Alarm Import Export Wizard to export the information to an XML file, or to import an alarm configuration XML file and create a new alarm configuration (MachineAlarms.MAL file) for an application.
Provide Feedback