Create Backup dialog box
When you select the
Import
option in the Alarm Import Export Wizard's Select Operation
dialog box, the Create Backup
dialog box opens. Backing up your present alarm configuration creates a well-formed XML file with the extension .bak.
IMPORTANT:
It is strongly recommended that you back up your existing alarm configuration before importing a new one.
TIP:
Click
No
and then Next
to proceed to the Select File
dialog box without backing up your present alarm configuration.Provide Feedback