Select Backup Destination dialog box
If you selected
Yes
in the Create Backup dialog box, the Select Backup Destination
dialog box opens. Use this dialog box to specify a name and a location for your backup configuration (.bak) file.Enter a name for the backup file
The default name for the backup alarm configuration file is
Alarms
. To use a different name, replace Alarms with the new name.Select where to store the backup file
The default location for the backup alarm configuration file is the root directory of the current application. To specify a different location, click the
Browse
button and navigate to the location you want to use. You can create a new folder if you need to.
TIP:
The backup file is not created until the new configuration file is imported.
Provide Feedback