Example: Alarm XML file
The structure of the ME Alarm XML file is given below. There are three main sections, alarms, triggers, and messages, which correlate to the
Advanced
, Triggers
, and Messages
tabs of the Alarm Setup
editor.Elements are in maroon text. Attributes are red. Values are blue.
<?xml version="1.0" encoding="UTF-8" ?> <alarms id="Alarms" version="1.0" product="{123-456-789}"> <alarm history-size="64" display-name="[ALARM]" hold-time="250" max-update- rate="0.5" silence-tag="" remote-silence-exp="" remote-ack-all-exp="" status-reset- tag="" remote-status-reset-exp="" close-display-tag="" remote-close-display-exp="" use- alarm-identifier="true"> <triggers> <trigger id="T1" type="value" ack-all-value="25" use-ack-all="true" ack-tag="" exp="if tag2 = 0 then 5 else if Tag2 = 1 then 10 else 15" message-tag="" message-handshake-exp="" message-notification-tag="" remote-ack-exp="" remote-ack-handshake-tag="" label="Label1" handshake-tag="" /> <trigger id="T2" type="bit" ack-all-value="0" use-ack-all="false" ack-tag="" exp="Tag1 = 20" message-tag="Alarm/Message1" message-handshake-exp="Alarm/Handshake1" message-notification-tag="Alarm/Notification1" remote-ack-exp="" remote-ack-handshake-tag="" label="" handshake-tag="HandshakeTag1" /> </triggers> <messages> <message id="M1" trigger-value="1" identifier="1" trigger="#T1" backcolor="#c00000" forecolor="#ffffff" audio="true" display="true" print="false" message-to-tag="true" text="Tank Full" /> <message id="M2" trigger-value="2" identifier="0" trigger="#T2" backcolor="#c00000" forecolor="#ffffff" audio="true" display="true" print="false" message-to-tag="true" text="Tank Overflow" /> </messages> </alarm> </alarms>
Provide Feedback