Export alarms

When you select the export operation in the
Alarm Import Export Wizard Select Operation
dialog box, the
Select Destination
dialog box opens. Specify the name of the exported alarm configuration file and where it will be stored.
To export the file
  • Click
    Finish
    .
The Alarm Import Export Wizard will generate a well-formed XML file containing the application's alarm configuration and store it in the location you specified. The file will have a .xml extension.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal