Alarm XML file elements
XML Declaration
An exported XML file begins with an XML declaration, containing the XML version and the encoding information.
An XML declaration is one of the following:
- <xml version="1.0" encoding="UTF-8 ?>
- <xml version="1.0" encoding="UTF-16 ?>
An XML declaration is optional for an import file.
If you are creating XML documents in Notepad, the files can be saved in UTF-8 or UTF-16 file format. (Notepad's Unicode file type corresponds to UTF-16 file format.) For files containing strings in English or other Latin-based languages, UTF-8 is recommended, to reduce the size of the xml file. For other foreign languages such as Chinese. Japanese or Korean, UTF-16 is recommended.
XML elements and attributes
In the following definitions, objects in braces <> indicate a data type such as string, int, float, and others.
Objects separated by | indicate the possible values for the attribute, only one of which is allowed.
Alarms element
The alarms element contains all attributes and elements in the XML file.
Alarms element attributes include the following:
- version= <float>
- id= <string> - optional
- product= <string> - optional
Alarm element
The alarm element must be contained within the alarms element. The alarm element corresponds to the
Advanced
tab of the ME Alarm Setup
editor. The Triggers element and the Messages element are nested within the alarm element.Alarm element attributes include the following:
- history-size= <int> (1 to 10000)
- display-name= <string>
- hold-time= 50 | 250 | 500 | 750 | 1000 | 2000 | 3000 | 4000 | 5000
- max-update-rate= 0.05 | 0.1 | .025 | 0.5 | 1 | 2 | 5 | 10 | 60 | 120
- silence-tag= <tag>
- remote-silence-exp= <tag or expression>
- remote-ack-all-exp= <tag or expression>
- status-reset-tag= <tag>
- remote-status-reset-exp =<tag or expression>
- close-display-tag= <tag>
- remote-close-display-exp= <tag or expression>
- use-alarm-identifier= true | false
Triggers element
The triggers element must be contained within the alarms element and within the alarm element. The triggers element corresponds to the
Triggers
tab of the Alarm Setup
editor. The "triggers" element will contain multiple "trigger" elements whose attributes define each trigger.Trigger element attributes include the following:
- id= <string>
- exp= <tag or expression>
- type= value | bit | lsbit
- label= <string> - this string cannot include a comma
- use-ack-all= true | false
- ack-all-value= <int> (-2147483648 to 2147483647)
- handshake-tag= <tag>
- ack-tag= <tag>
- remote-ack-exp= <tag or expression>
- remote-ack-handshake-tag= <tag>
- message-tag= <tag>
- message-notification-tag= <tag>
- message-handshake-exp= <tag or expression>
Messages element
The messages element must be contained within the alarms element and within the alarm element. This element corresponds to the
Messages
tab of the Alarm Setup
editor.Messages element attributes include the following:
- id= <string> - optional
- trigger-value= <int> (-2147483648 to 2147483647)
- identifier= <int> (0 to - 32767)
- trigger= #<T> | all | "" - enter a # character followed by the ID number of the trigger that is triggering the message. OR all to use the <AllTriggers>, OR "" to indicate <Unassigned>.
- backcolor= <color> - enter a # character followed by the RRGGBB value of the color.
- forecolor= <color> - enter a # character followed by the RRGGBB value of the color.
- audio= true | false
- display= true | false
- print= true | false
- message-to-tag= true | false
- text= <string>
Provide Feedback