Alarm Import Export Wizard select operation
When the Alarm Import Export Wizard opens, specify whether you want to export the alarm configuration from an application or import alarm configuration into an application.
Export alarm configuration from application
Click this button to export the alarm configuration in the application's MachineAlarms.MAL file to an XML file.
Import alarm configuration into application
Click this button to import an XML file and create a new alarm configuration (MachineAlarms.MAL file) for the application from the information in the XML file. The existing alarm configuration file will be overwritten.
Provide Feedback