Language switching

Language switching allows you to deploy an application in different languages. At design time, you can design an application with user-defined text strings in up to 40 languages. At runtime, you can switch between up to 20 application languages dynamically using a language switch button for each language.
The user-defined text strings that support language switching are those that an operator sees in an application at runtime, including:
  • Text objects created in graphic displays and global object displays
  • Graphic and global object display titles specified in the
    Display Settings
    dialog box
  • Labels and captions on graphic displays, including alarm trigger labels
  • Embedded time and date and numeric variables
  • Alarm, local, and information messages
  • Captions and shorter messages in the dialog boxes of
    User Management
    buttons and the
    Electronic Signature
    dialog box
  • Text strings defined in the extended properties of controller tags
    TIP:
    Make sure that you define the controller default language when multi-language is enabled.
    • If the requested language is not available in the controller, the application shows the default language defined and enabled in the HMI.
    • If the HMI default language is not defined in the controller, the application uses the controller default language or the single language that does not have an ID.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal