Add a language to an application

Use the
Add
button on the
General
tab of the
Language Configuration
dialog box to add a language to an application.
The language list in the
Add Language
dialog box shows the languages supported by the design-time computer running
FactoryTalk View Studio
.
To add a language to an application
  1. In the
    Language Configuration
    dialog box, click
    Add
    .
  2. In the
    Add Language
    dialog box, select the language to be added to the application and click
    OK.
The
Add Language dialog
box closes and the selected language is added to the list on the
General
tab.
TIP:
The languages in the
Add Language
dialog box are those supported by the operating system of the computer. They are not necessarily installed on the computer. If the selected language is not installed, a warning message appears in the
Diagnostics
List
at the bottom of the Explorer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal