Default language
When you create an application, the language you select in the
New/Open Machine Edition Application
dialog box becomes the default language for the application. Any undefined strings in the application can be shown in the default language rather than as question marks.When you open an existing application that supports only one language, that language is the default language.
When you open an existing application that supports multiple languages, the language you select to open the application in becomes the application's current language. Once the application is opened, you can change the default language in the
Language Configuration
dialog box.When you open an existing application created with RSView Studio Machine Edition 4.00 in
FactoryTalk View Studio
, if the application supports multiple languages, you are prompted to select a default language for the application.Provide Feedback