Windows locale formatting and fonts
To switch application languages, you may need set up Windows locale formatting and fonts.
Locale formatting
Windows locale formatting determines how the application shows time, date, and floating point values at design time and runtime.
It is strongly recommended that you do not edit the default locale settings for the following reasons:
- You can only modify the formatting for the current user locale. The formatting for all other locales is set to their default values. For example, if you select English (United States) as the current user locale, modify its formats, and then select another locale, the modifications will be lost.
- You can only modify settings for the current user. If more than one user will be logged in, they will all have to make the same modifications.
- You can only modify locale settings for languages that are installed.TIP:Locale formatting is supported onPanelView Plus 7andPanelView Plus 6terminals, but is not supported onPanelView PlusorPanelView Plus CEterminals.When the application language is switched, the default locale settings for the new language are used even if that language is not installed.
Fonts
Windows font support features allow an application to show characters that are not supported by the application's original font. If the application text strings are exported and translated into Chinese, for example, and then re-imported, the translated text will show in the Chinese font without the necessity of changing the font selection in every instance in the application.
Font support is enabled automatically when you install a language or language group. Once you install the East Asian language group, for example, fonts for these languages, including Chinese, are supported. If font support is disabled, any characters that the font cannot show will appear as undefined "?" characters.
TIP:
On
Windows
computers, some raster fonts, those with a .fon extension, and fonts with a symbol script, (for example, Wingdings), do not show characters from other fonts.FactoryTalk View ME
Station supports font linking for PanelView Plus 7
, PanelView Plus 6
, PanelView Plus
, and PanelView Plus CE
terminals. Use the Font Linking
menu in FactoryTalk View ME Station
Terminal Settings
options to select a base font and to link another font to the base font. The base font and the linked font must be loaded on the terminal.If your runtime application uses fonts that are not installed with
FactoryTalk View ME Station
, you will need to either copy the fonts manually to the internal card of the terminals, or, if the font is too large for the terminal's memory, (as is, for example, the Simsun font), you can copy the font onto an external Compact Flash card. If an external Flash card is used, it will need to be plugged into the terminal at all times while the application is running.Provide Feedback