Set a registry key for font linking
To ensure that font linking works, it is recommended that you use Tahoma or Microsoft Sans Serif fonts in your
FactoryTalk View ME
application.To use language switching with another font, add a registry key for that font. You can link the base font to all the fonts that are linked to Tahoma or Microsoft Sans Serif.
The registry key that is set using these directions only exists when the fonts that support font linking are installed. When you install a new Windows language or language group, part of the process installs the fonts and enables font linking.
To link a base font to multiple fonts
- From WindowsStartmenu, selectRun.
- In theRundialog box, typeregedt32and pressOK.
- SelectComputer\HKEY_LOCAL_MACHINE\SOFTWARE\Microsoft\Windows NT\CurrentVersion\Fonts.
- In the right pane, double-clickTahomaorMicrosoft San Serif, and copy (Ctrl+C) the value data.
- SelectEdit > New > Multi-String Value.
- Right-click the new value, selectRename, and then type the name of the font that you want to set up font linking for, for example,Arial.
- In theValue databox, paste (Ctrl+V) the value you copied in step 4, and then clickOK.
When you restart the computer, the new font will be linked to all the fonts that Tahoma or Microsoft San Serif are linked to.
Provide Feedback