Show undefined text in the default language

You may need show the undefined text in the default language instead of question marks.
To show undefined text in the default language
  1. In the
    Language Configuration
    dialog box, select the
    Display undefined strings using the default language
    check box.
  2. Click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal