- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
CheckBox style
Properties
Name | BrowseName | DataType | Description |
---|---|---|---|
Indicator size | IndicatorSize | ||
Text color | TextColor | Color of the text to display | |
Active background color | ActiveBackgroundColor | Background color of the element while is active | |
Active text color | ActiveTextColor | Text color of the element while is active | |
Active tick color | ActiveTickColor | Tick color of the element while is active | |
Font family | FontFamily | Font family | |
Font weight | FontWeight | Font weight | |
Font italic | FontItalic | Enables/disables italics in the text | |
Font size | FontSize | Font size | |
Radius | Radius | Radius of the angles of the objects |
Provide Feedback