Keyboard shortcuts

FactoryTalk Optix Studio
supports these keyboard shortcuts.

Global

Global keyboard shortcuts
Shortcut
Description
Open
FactoryTalk Optix
Help.
+
Copy the selected item.
+
Paste the copied item into the selected location.
+
Undo previous action.
+
Redo previous action.
+
Save the current
FactoryTalk Optix Application
project.
Run
FactoryTalk Optix Application
. For more information, see Deploy a FactoryTalk Optix Application.
+
+
Find text in the current project. For more information, see Find text in a project.
+
+
Find and replace text in the current project. For more information, see Replace text in a project.
Delete the selected item.
Discard edits or close a dialog.
+
Add a new line.
Interact with the selected item.

Panes

The following shortcuts apply to panes in
FactoryTalk Optix Studio
. For more information about
FactoryTalk Optix Studio
panes, see FactoryTalk Optix Studio GUI.
Panes shortcuts
Shortcut
Description
Select previous item.
Select next item.
Expand the selected item.
Collapse the selected item.
+
Select the previously selected item in
Project view
. For more information, see Project view.
+
Select the next item in
Project view
. For more information, see Project view.
+ left mouse click
Select all items between the selected item and the clicked item.
Rename the selected item.

Localization dictionary

For more information about localization dictionaries and strings translation, see Localization editor.
Localization dictionary shortcuts
Shortcut
Description
+
Select all keys and values in the translation table.

UI editor

The following shortcuts apply to the editor that allows you to arrange graphic objects and create user interfaces for
FactoryTalk Optix Applications
. For more information, see Editor.
UI editor shortcuts
Shortcut
Description
Move the selected object up on the grid.
Move the selected object down on the grid.
Move the selected object left on the grid.
Move the selected object right on the grid.
+
Move the selected object up and align the object to the grid.
+
Move the selected object down and align the object to the grid.
+
Move the selected object left and align the object to the grid.
+
Move the selected object right and align the object to the grid.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal