MQTT Publisher
Allows to publish messages to MQTT Broker defined topic. Any MQTT client subscribed to that topic receives the messages
Properties
Name | BrowseName | DataType | Description |
---|---|---|---|
Sampling mode | SamplingMode | None - automatic recording disabled, can record by invoking the Sample method. Periodic - at regular intervals records the values of all the selected variables. Value change - at regular intervals records only the values of the selected variables that have changed since the previous sampling | |
Sampling period | SamplingPeriod | Interval in hours, with millisecond precision, between one sampling and the next, in the Periodic mode | |
Polling time | PollingPeriod | Interval in hours, with millisecond precision, between one sampling and the next, in the Value change mode | |
QoS | QoS | MQTT Quality of Service, defines the guarantee of delivery for a specific message (0, 1, 2). 0 - At most once (may lose messages). 1 - At least once (guarantees the message delivery but potentially duplicate messages). 2 - Exactly once (ensures messages are delivered exactly once without duplication) | |
Retain | Retain | Retain message on the topic even after read. True - enables Retain functionality. False - disables Retain functionality | |
PF Enabled | PFEnabled | True - enables payload formatter. False - disables payload formatter, default format is used | |
PF Header | PFHeader | Defines the header template in MQTT payload. See Help for details and examples | |
PF Record | PFRecord | Defines the record template for each record in MQTT payload. See Help for details and examples | |
Provide Feedback